Can we use i.MX6DQ IPU unpacking capability when input format is generic data.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can we use i.MX6DQ IPU unpacking capability when input format is generic data.

跳至解决方案
1,701 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our patner have a question about i.MX6DQ IPU.
Please see page 2732 in IMX6DQRM Rev.2.
It says "Unpacking and companding capabilities are provided for up to two streams (either through same or different interfaces), while the other ones are treated as generic data."
Then, can we use this function when input data as "generic data" (when CSIx_SENS_DATA_FORMAT = 011b)?


Best Regards,
Satoshi Shimoda

标记 (1)
0 项奖励
回复
1 解答
1,545 次查看
Yuri
NXP Employee
NXP Employee

Unpacking and companding capabilities are not provided for the generic data.

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,546 次查看
Yuri
NXP Employee
NXP Employee

Unpacking and companding capabilities are not provided for the generic data.

Regards,

Yuri.

0 项奖励
回复
1,545 次查看
satoshishimoda
Senior Contributor I

Hi Yuri,

I found the packing (companding) function in chapter 37.4.3.7 and Table 37-17 in IMX6DQRM Rev.3.

Bayer and Generic input data seem to be able to compand also according to this section, is this wrong?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1,545 次查看
Yuri
NXP Employee
NXP Employee

Hi,

  Basically, data unpacking means that format of data is known (say, R8G8B8).

For generic data, format is not predefined. The Table 37-17 states that generic

are treated just as bytes or 16-bit words, based on port size.

Regards,

Yuri.

0 项奖励
回复