Can we use i.MX6DQ IPU unpacking capability when input format is generic data.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we use i.MX6DQ IPU unpacking capability when input format is generic data.

ソリューションへジャンプ
1,690件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our patner have a question about i.MX6DQ IPU.
Please see page 2732 in IMX6DQRM Rev.2.
It says "Unpacking and companding capabilities are provided for up to two streams (either through same or different interfaces), while the other ones are treated as generic data."
Then, can we use this function when input data as "generic data" (when CSIx_SENS_DATA_FORMAT = 011b)?


Best Regards,
Satoshi Shimoda

ラベル(5)
タグ(1)
0 件の賞賛
返信
1 解決策
1,534件の閲覧回数
Yuri
NXP Employee
NXP Employee

Unpacking and companding capabilities are not provided for the generic data.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,535件の閲覧回数
Yuri
NXP Employee
NXP Employee

Unpacking and companding capabilities are not provided for the generic data.

Regards,

Yuri.

0 件の賞賛
返信
1,534件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Yuri,

I found the packing (companding) function in chapter 37.4.3.7 and Table 37-17 in IMX6DQRM Rev.3.

Bayer and Generic input data seem to be able to compand also according to this section, is this wrong?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,534件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

  Basically, data unpacking means that format of data is known (say, R8G8B8).

For generic data, format is not predefined. The Table 37-17 states that generic

are treated just as bytes or 16-bit words, based on port size.

Regards,

Yuri.

0 件の賞賛
返信