Can we modify suspend ram sections in power mode switch example to be smaller? [imx7ulp]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we modify suspend ram sections in power mode switch example to be smaller? [imx7ulp]

1,904 Views
cervenka
Contributor III

Hello,

we wanted run in VLLS mode on A7 and M4 core. We are using RAM target for m4, but m_text region is not enough for us. I was curious if we can move some space from m_m4_suspend_ram/m_a7_suspend_ram regions to m_text region. I see that some part of RAM is stored there and then restored as a result of ROM may overwrite specific part of RAM (but don't see how much and where). 

QSPI memory is used for permanent storing/logging data from m4 core.

Labels (1)
0 Kudos
Reply
1 Reply

1,872 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can modify the RAM space with the linker file, however you can not with ROM space.

Regards

0 Kudos
Reply