Can we modify suspend ram sections in power mode switch example to be smaller? [imx7ulp]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we modify suspend ram sections in power mode switch example to be smaller? [imx7ulp]

1,878件の閲覧回数
cervenka
Contributor III

Hello,

we wanted run in VLLS mode on A7 and M4 core. We are using RAM target for m4, but m_text region is not enough for us. I was curious if we can move some space from m_m4_suspend_ram/m_a7_suspend_ram regions to m_text region. I see that some part of RAM is stored there and then restored as a result of ROM may overwrite specific part of RAM (but don't see how much and where). 

QSPI memory is used for permanent storing/logging data from m4 core.

ラベル(1)
0 件の賞賛
返信
1 返信

1,846件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can modify the RAM space with the linker file, however you can not with ROM space.

Regards

0 件の賞賛
返信