Hello,
i have some board with iMX6Q
There i have the U-boot menu.
By default systems start with this parameters:
setenv bootargs console=ttySAC0,115200 init=/init video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB24,bpp=32 ldb=spl0 video=mxcfb1:off video=mxcfb2:off fbmem=48M vmalloc=400M androidboot.console=ttySAC0 androidboot.hardware=freescale
i trying to change the LVDS output from 24bit to 18bit.
It's mean i need to change RGB24 to RGB666.
setenv bootargs console=ttySAC0,115200 init=/init video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB666,bpp=32 ldb=spl0 video=mxcfb1:off video=mxcfb2:off fbmem=48M vmalloc=400M androidboot.console=ttySAC0 androidboot.hardware=freescale
Next step: saveenv
i see this:
Saving Environment to MMC...
Writing to MMC(3)... done
Right?
but on next step i run Boot, and in log i see it's run with default parametrs RGB24. it's mean not saved my parametrs. Why so?
Next step: boot or run bootcmd
How to change this parametrs? why his not saved the new parametrs?
And another quastion:
There i have boot menu
[1]boot from emmc
[2]boot from sdcard
[3]boot from tftp
[5]download from sdcard
[0]setting boot args
[q]exit to command mode
Enter your selection:
How to change thismenu and parametrs?
Thank's lot,
Andrey
已解决! 转到解答。
Hi Andrey
if this is not Freescale board and software
suggest to post this on Uboot mailing list and software vendor forum
UBootEnvVariables < DULG < DENX
Best regards
igor
Hi Andrey
if this is not Freescale board and software
suggest to post this on Uboot mailing list and software vendor forum
UBootEnvVariables < DULG < DENX
Best regards
igor