Can't save parameters in U-Boot (iMX6Q)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't save parameters in U-Boot (iMX6Q)

ソリューションへジャンプ
1,406件の閲覧回数
andreylipov
Contributor II

Hello,

i have some board with iMX6Q

There i have the U-boot menu.

By default systems start with this parameters:

setenv bootargs console=ttySAC0,115200 init=/init video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB24,bpp=32 ldb=spl0 video=mxcfb1:off video=mxcfb2:off fbmem=48M vmalloc=400M androidboot.console=ttySAC0 androidboot.hardware=freescale

i trying to change the LVDS output from 24bit to 18bit.

It's mean i need to change RGB24 to RGB666.

setenv bootargs console=ttySAC0,115200 init=/init video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB666,bpp=32 ldb=spl0 video=mxcfb1:off video=mxcfb2:off fbmem=48M vmalloc=400M androidboot.console=ttySAC0 androidboot.hardware=freescale

Next step: saveenv

i see this:

Saving Environment to MMC...

Writing to MMC(3)... done

Right?

but on next step i run Boot, and in log i see it's run with default parametrs RGB24. it's mean not saved my parametrs. Why so?

Next step: boot or run bootcmd

How to change this parametrs? why his not saved the new parametrs?

And another quastion:

There i have boot menu

[1]boot from emmc

[2]boot from sdcard

[3]boot from tftp

[5]download from sdcard

[0]setting boot args

[q]exit to command mode

Enter your selection:

How to change thismenu and parametrs?

Thank's lot,

Andrey

ラベル(3)
0 件の賞賛
返信
1 解決策
1,175件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrey

if this is not Freescale board and software

suggest to post this on Uboot mailing list and software vendor forum

UBootEnvVariables < DULG < DENX

U-Boot Info Page

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,176件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrey

if this is not Freescale board and software

suggest to post this on Uboot mailing list and software vendor forum

UBootEnvVariables < DULG < DENX

U-Boot Info Page

Best regards

igor

0 件の賞賛
返信