Can i use EIM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can i use EIM?

跳至解决方案
1,106 次查看
hanseunglee
Contributor III

My configure set below,

--------------------------------------------------------------------------------

YOCTO

kernel : 3.14.52

i.mx6dl sabresd

ununtu 14.04

--------------------------------------------------------------------------------

EIM max frequency 133Mhz...

According to fig.22-5 , real data rate  is 133/6 Mhz for data transfer?  = 22Mhz?

How to think about EIM timing chart?

I will use multiplexed address/data mode - 16bit. Can i use more fast clock than 22Mhz?

pastedImage_2.png

pastedImage_1.png

标签 (1)
0 项奖励
回复
1 解答
1,024 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Most effective approach is using burst mode, where data can be accessed every

burst clock. In such way maximum frequency of 133 MHz may be achieved with EIM

during bust.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,025 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Most effective approach is using burst mode, where data can be accessed every

burst clock. In such way maximum frequency of 133 MHz may be achieved with EIM

during bust.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复