Can i use EIM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,602件の閲覧回数
hanseunglee
Contributor III

My configure set below,

--------------------------------------------------------------------------------

YOCTO

kernel : 3.14.52

i.mx6dl sabresd

ununtu 14.04

--------------------------------------------------------------------------------

EIM max frequency 133Mhz...

According to fig.22-5 , real data rate  is 133/6 Mhz for data transfer?  = 22Mhz?

How to think about EIM timing chart?

I will use multiplexed address/data mode - 16bit. Can i use more fast clock than 22Mhz?

pastedImage_2.png

pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
1 解決策
1,520件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Most effective approach is using burst mode, where data can be accessed every

burst clock. In such way maximum frequency of 133 MHz may be achieved with EIM

during bust.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,521件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Most effective approach is using burst mode, where data can be accessed every

burst clock. In such way maximum frequency of 133 MHz may be achieved with EIM

during bust.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信