Can i use EIM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i use EIM?

Jump to solution
792 Views
hanseunglee
Contributor III

My configure set below,

--------------------------------------------------------------------------------

YOCTO

kernel : 3.14.52

i.mx6dl sabresd

ununtu 14.04

--------------------------------------------------------------------------------

EIM max frequency 133Mhz...

According to fig.22-5 , real data rate  is 133/6 Mhz for data transfer?  = 22Mhz?

How to think about EIM timing chart?

I will use multiplexed address/data mode - 16bit. Can i use more fast clock than 22Mhz?

pastedImage_2.png

pastedImage_1.png

Labels (1)
0 Kudos
Reply
1 Solution
710 Views
Yuri
NXP Employee
NXP Employee

Hello,

Most effective approach is using burst mode, where data can be accessed every

burst clock. In such way maximum frequency of 133 MHz may be achieved with EIM

during bust.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
711 Views
Yuri
NXP Employee
NXP Employee

Hello,

Most effective approach is using burst mode, where data can be accessed every

burst clock. In such way maximum frequency of 133 MHz may be achieved with EIM

during bust.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply