Can PCIE be used to receive LVDS data with imx6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can PCIE be used to receive LVDS data with imx6?

跳至解决方案
2,531 次查看
Simon_Wu00
Contributor II

Hi,

    I found that PCIE uses LVDS to transmit data.Can PCIE be used to receive LVDS data?

    I want to use dp to lvds chip to convert the DP signal, and use the PCIE of MX6 to receive it. Is this feasible?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,505 次查看
igorpadykov
NXP Employee
NXP Employee

yes, if custom driver will comply with protocols defined in PCIe specification.

Also HCSL logic is used for PCIe, description can be found for example in

https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,527 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Simon

 

I am afraid it is not feasible, as i.MX6Q PCIe module works only with devices compatible with PCIe

specification :  https://en.wikipedia.org/wiki/PCI_Express

https://www.electronicdesign.com/technologies/communications/article/21762833/pci-express-and-the-ph...

also may be helpful

https://community.nxp.com/t5/i-MX-Processors/i-mx6Q-PCIe-clock/m-p/802364/highlight/true

 

Best regards
igor

0 项奖励
回复
2,521 次查看
Simon_Wu00
Contributor II

Hi igor,

If I write my own LVDS driver, can I use MIPI-CSI or PCIE interface to receive LVDS?

 

Best regards

Simon

0 项奖励
回复
2,506 次查看
igorpadykov
NXP Employee
NXP Employee

yes, if custom driver will comply with protocols defined in PCIe specification.

Also HCSL logic is used for PCIe, description can be found for example in

https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en

 

Best regards
igor

0 项奖励
回复