Can PCIE be used to receive LVDS data with imx6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can PCIE be used to receive LVDS data with imx6?

Jump to solution
1,004 Views
Simon_Wu00
Contributor II

Hi,

    I found that PCIE uses LVDS to transmit data.Can PCIE be used to receive LVDS data?

    I want to use dp to lvds chip to convert the DP signal, and use the PCIE of MX6 to receive it. Is this feasible?

Labels (1)
Tags (1)
0 Kudos
1 Solution
978 Views
igorpadykov
NXP Employee
NXP Employee

yes, if custom driver will comply with protocols defined in PCIe specification.

Also HCSL logic is used for PCIe, description can be found for example in

https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en

 

Best regards
igor

View solution in original post

0 Kudos
3 Replies
1,000 Views
igorpadykov
NXP Employee
NXP Employee

Hi Simon

 

I am afraid it is not feasible, as i.MX6Q PCIe module works only with devices compatible with PCIe

specification :  https://en.wikipedia.org/wiki/PCI_Express

https://www.electronicdesign.com/technologies/communications/article/21762833/pci-express-and-the-ph...

also may be helpful

https://community.nxp.com/t5/i-MX-Processors/i-mx6Q-PCIe-clock/m-p/802364/highlight/true

 

Best regards
igor

0 Kudos
994 Views
Simon_Wu00
Contributor II

Hi igor,

If I write my own LVDS driver, can I use MIPI-CSI or PCIE interface to receive LVDS?

 

Best regards

Simon

0 Kudos
979 Views
igorpadykov
NXP Employee
NXP Employee

yes, if custom driver will comply with protocols defined in PCIe specification.

Also HCSL logic is used for PCIe, description can be found for example in

https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en

 

Best regards
igor

0 Kudos