Can PCIE be used to receive LVDS data with imx6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can PCIE be used to receive LVDS data with imx6?

ソリューションへジャンプ
2,476件の閲覧回数
Simon_Wu00
Contributor II

Hi,

    I found that PCIE uses LVDS to transmit data.Can PCIE be used to receive LVDS data?

    I want to use dp to lvds chip to convert the DP signal, and use the PCIE of MX6 to receive it. Is this feasible?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,450件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes, if custom driver will comply with protocols defined in PCIe specification.

Also HCSL logic is used for PCIe, description can be found for example in

https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,472件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Simon

 

I am afraid it is not feasible, as i.MX6Q PCIe module works only with devices compatible with PCIe

specification :  https://en.wikipedia.org/wiki/PCI_Express

https://www.electronicdesign.com/technologies/communications/article/21762833/pci-express-and-the-ph...

also may be helpful

https://community.nxp.com/t5/i-MX-Processors/i-mx6Q-PCIe-clock/m-p/802364/highlight/true

 

Best regards
igor

0 件の賞賛
返信
2,466件の閲覧回数
Simon_Wu00
Contributor II

Hi igor,

If I write my own LVDS driver, can I use MIPI-CSI or PCIE interface to receive LVDS?

 

Best regards

Simon

0 件の賞賛
返信
2,451件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes, if custom driver will comply with protocols defined in PCIe specification.

Also HCSL logic is used for PCIe, description can be found for example in

https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en

 

Best regards
igor

0 件の賞賛
返信