Cache snooping and DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cache snooping and DMA

Jump to solution
1,873 Views
sabine_s
Contributor III

Is there a DMA controller on the i.MX8QM that can move data between main memory and a peripheral while simultaneously snooping the cache when moving from memory to peripheral and/or creating new cache entries when moving from peripheral to main memory?

Some of the older QorIQ PowerPC processors had this feature and it sped up our application a great deal and I am hoping there is an equivalent for the i.MX8QM.

0 Kudos
Reply
1 Solution
1,868 Views
b36401
NXP Employee
NXP Employee

i.MX8 has no such mechanism. Sorry for the inconvenience.

View solution in original post

0 Kudos
Reply
1 Reply
1,869 Views
b36401
NXP Employee
NXP Employee

i.MX8 has no such mechanism. Sorry for the inconvenience.

0 Kudos
Reply