Cache snooping and DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cache snooping and DMA

ソリューションへジャンプ
1,861件の閲覧回数
sabine_s
Contributor III

Is there a DMA controller on the i.MX8QM that can move data between main memory and a peripheral while simultaneously snooping the cache when moving from memory to peripheral and/or creating new cache entries when moving from peripheral to main memory?

Some of the older QorIQ PowerPC processors had this feature and it sped up our application a great deal and I am hoping there is an equivalent for the i.MX8QM.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,856件の閲覧回数
b36401
NXP Employee
NXP Employee

i.MX8 has no such mechanism. Sorry for the inconvenience.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,857件の閲覧回数
b36401
NXP Employee
NXP Employee

i.MX8 has no such mechanism. Sorry for the inconvenience.

0 件の賞賛
返信