CCM_CLKO as CLK input for peripheral

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCM_CLKO as CLK input for peripheral

Jump to solution
6,390 Views
thorben
Contributor II

Hi,

on the iMX8M mini, can we use CCM_CLKO from Clock Control Module (CCM) as an input clock for some external peripheral on our PCB or is CCM_CLKO just meant to be a test/control clock output and not intended to serve as an input clock?

Regards,

Thorben

Labels (1)
0 Kudos
Reply
1 Solution
6,180 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hello, I got the update from our expert team.

Checked with our SOC, it's not recomended to drive external device by CLKOUT. Jitter may also relate to PCB layout.

The CLKOUT is not designed for the purpose. It's just for monitor.

Hope this can do help for you.

Have a nice day

Rita

View solution in original post

0 Kudos
Reply
7 Replies
6,180 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which product are you using?

0 Kudos
Reply
6,180 Views
thorben
Contributor II

I'm sorry, I only added the processor type to the tags. It's a iMX8M mini.

0 Kudos
Reply
6,176 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I got the update from our expert, Please refer to the register definition. OFFSET: 0x128

0 Kudos
Reply
6,176 Views
thorben
Contributor II

Thank you. I already know these values from the reference manual. I want to know if we can use it as an clock input for external peripheral? Does this output have for example jitter? If it's just a monitor clock and it maybe has some jitter, we wouldn't be able to use it.

0 Kudos
Reply
6,181 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hello, I got the update from our expert team.

Checked with our SOC, it's not recomended to drive external device by CLKOUT. Jitter may also relate to PCB layout.

The CLKOUT is not designed for the purpose. It's just for monitor.

Hope this can do help for you.

Have a nice day

Rita

0 Kudos
Reply
6,176 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

We are confirming it for you.

0 Kudos
Reply
6,176 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I have sent your question to our expert team, when I get update I will send to you as soon as possible.

0 Kudos
Reply