Boot i.MX8M with DDR4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Boot i.MX8M with DDR4

跳至解决方案
1,574 次查看
lizboxy
Contributor I

Hi,Sir:

We are debugging i.MX8M with DDR4, and passed the DDR Stress Test in attached.But i.MX8M is still in resetting  when checking the  log as below.

From the log, I guess that: just fix the config of DDR4, not the FW of DDR4, then download the FW of LPDDR4 after reset.  So how to fix the FW of LPDDR4 with DDR4? 

And checking the DDR Tool User guide, not only copy the DDR4_timing to board/freescale/imx8mq_evk/ ,

but also need to copy the FW of DDR4 to image ,but how to compile?

0 项奖励
回复
1 解答
1,566 次查看
Yuri
NXP Employee
NXP Employee

@lizboxy 
Hello,

  use

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

MSCALE_DDR_Tool_User_Guide  (in the DDR Tool package) describes how to add
support for new memory, in particular section 4.3 (Building u-boot image) explains
how to build all the needed software.

 

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,567 次查看
Yuri
NXP Employee
NXP Employee

@lizboxy 
Hello,

  use

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

MSCALE_DDR_Tool_User_Guide  (in the DDR Tool package) describes how to add
support for new memory, in particular section 4.3 (Building u-boot image) explains
how to build all the needed software.

 

Regards,
Yuri.

0 项奖励
回复