Boot i.MX8M with DDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot i.MX8M with DDR4

Jump to solution
1,554 Views
lizboxy
Contributor I

Hi,Sir:

We are debugging i.MX8M with DDR4, and passed the DDR Stress Test in attached.But i.MX8M is still in resetting  when checking the  log as below.

From the log, I guess that: just fix the config of DDR4, not the FW of DDR4, then download the FW of LPDDR4 after reset.  So how to fix the FW of LPDDR4 with DDR4? 

And checking the DDR Tool User guide, not only copy the DDR4_timing to board/freescale/imx8mq_evk/ ,

but also need to copy the FW of DDR4 to image ,but how to compile?

0 Kudos
Reply
1 Solution
1,546 Views
Yuri
NXP Employee
NXP Employee

@lizboxy 
Hello,

  use

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

MSCALE_DDR_Tool_User_Guide  (in the DDR Tool package) describes how to add
support for new memory, in particular section 4.3 (Building u-boot image) explains
how to build all the needed software.

 

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
1,547 Views
Yuri
NXP Employee
NXP Employee

@lizboxy 
Hello,

  use

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

MSCALE_DDR_Tool_User_Guide  (in the DDR Tool package) describes how to add
support for new memory, in particular section 4.3 (Building u-boot image) explains
how to build all the needed software.

 

Regards,
Yuri.

0 Kudos
Reply