Boot i.MX8M with DDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot i.MX8M with DDR4

ソリューションへジャンプ
1,563件の閲覧回数
lizboxy
Contributor I

Hi,Sir:

We are debugging i.MX8M with DDR4, and passed the DDR Stress Test in attached.But i.MX8M is still in resetting  when checking the  log as below.

From the log, I guess that: just fix the config of DDR4, not the FW of DDR4, then download the FW of LPDDR4 after reset.  So how to fix the FW of LPDDR4 with DDR4? 

And checking the DDR Tool User guide, not only copy the DDR4_timing to board/freescale/imx8mq_evk/ ,

but also need to copy the FW of DDR4 to image ,but how to compile?

0 件の賞賛
返信
1 解決策
1,555件の閲覧回数
Yuri
NXP Employee
NXP Employee

@lizboxy 
Hello,

  use

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

MSCALE_DDR_Tool_User_Guide  (in the DDR Tool package) describes how to add
support for new memory, in particular section 4.3 (Building u-boot image) explains
how to build all the needed software.

 

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,556件の閲覧回数
Yuri
NXP Employee
NXP Employee

@lizboxy 
Hello,

  use

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

MSCALE_DDR_Tool_User_Guide  (in the DDR Tool package) describes how to add
support for new memory, in particular section 4.3 (Building u-boot image) explains
how to build all the needed software.

 

Regards,
Yuri.

0 件の賞賛
返信