Boot from usb disk hardware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Boot from usb disk hardware

跳至解决方案
1,613 次查看
zh_y
Contributor II

My board platform is i.MX6QP .I want to start uboot, kernel and rootfs from usb disk hardware. Is there any good way?

0 项奖励
回复
1 解答
1,489 次查看
diegoadrian
NXP Employee
NXP Employee

Unfortunately,

That is impossible, the only boot devices for the i.MX6Q are the following ones:

• NOR flash
• NAND flash
• OneNAND flash
• SD/MMC
• Serial ATA (SATA) HDD (only i.MX 6Dual/6Quad)
• Serial (I2C/SPI) NOR flash and EEPROM

Best regards,

Diego.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,490 次查看
diegoadrian
NXP Employee
NXP Employee

Unfortunately,

That is impossible, the only boot devices for the i.MX6Q are the following ones:

• NOR flash
• NAND flash
• OneNAND flash
• SD/MMC
• Serial ATA (SATA) HDD (only i.MX 6Dual/6Quad)
• Serial (I2C/SPI) NOR flash and EEPROM

Best regards,

Diego.

0 项奖励
回复