Boot from usb disk hardware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot from usb disk hardware

Jump to solution
2,257 Views
zh_y
Contributor II

My board platform is i.MX6QP .I want to start uboot, kernel and rootfs from usb disk hardware. Is there any good way?

0 Kudos
Reply
1 Solution
2,133 Views
diegoadrian
NXP Employee
NXP Employee

Unfortunately,

That is impossible, the only boot devices for the i.MX6Q are the following ones:

• NOR flash
• NAND flash
• OneNAND flash
• SD/MMC
• Serial ATA (SATA) HDD (only i.MX 6Dual/6Quad)
• Serial (I2C/SPI) NOR flash and EEPROM

Best regards,

Diego.

View solution in original post

0 Kudos
Reply
1 Reply
2,134 Views
diegoadrian
NXP Employee
NXP Employee

Unfortunately,

That is impossible, the only boot devices for the i.MX6Q are the following ones:

• NOR flash
• NAND flash
• OneNAND flash
• SD/MMC
• Serial ATA (SATA) HDD (only i.MX 6Dual/6Quad)
• Serial (I2C/SPI) NOR flash and EEPROM

Best regards,

Diego.

0 Kudos
Reply