LBEE5KL1DX wifi-ble module SDIO, CLK & CMD length matching(+/- for PCB design).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LBEE5KL1DX wifi-ble module SDIO, CLK & CMD length matching(+/- for PCB design).

1,980 Views
prabhu1
Contributor III

Hi Sir/Mam,

Please, Could you give suggestions on LBEE5KL1DX wifi-ble module SDIO, CLK & CMD length matching(+/- for PCB design).

 

With Regards,

K Prabhu Kumar.

8050415207,

Bangalore,

India.

Labels (1)
3 Replies

1,881 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prabhu

for SD/SDIO routing guidelines one can refer to sect.3.6.8High speed signal routing recommendations

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,881 Views
prabhu1
Contributor III

Hi Igor,

Thanks for your reply.

In my design I interfaced LBEE5KL1DX Murata WIFI-BLE module and I.MX6ULL.

So, What is the minimum trace length tolerance(+/-) between SDIO,CLK & CMD lines in PCB.

Currently I kept 150mil +/- .

0 Kudos
Reply

1,881 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prabhu

 

sect.3.6.8 High speed signal routing recommendations is also applicable

to that case.

Best regards
igor

0 Kudos
Reply