BitBlit function on GC320 in i.MX6SDL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BitBlit function on GC320 in i.MX6SDL.

ソリューションへジャンプ
2,106件の閲覧回数
keitanagashima
Senior Contributor I

Hi.

I'd like to use the BitBlit function on GC320 of i.MX6SDL in Linux.

When using the feature of 2D BitBlit, I think that the Vivante's API must be used.

To use the API of Vivante, the header file of Vivante becomes necessary.

Is it possible to get the source code of the graphics function of Vivante?

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
1,509件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, 2D functions can be used please refer to

i.MX_6_G2D_API_User's_Guide.pdf included in

Linux documentation

"L3.10.17_1.0.0_IMX6QDLS_BUNDLE  : Source Code Download Steps Documentation and Demo Images."

i.MX6Q: i.MX 6Quad Family of Applications Processors

Best regards

chip

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,509件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Freescale does not provide GPU drivers sources because they are license protected.

Sources should be obtained only through local Freescale marketing channel.

0 件の賞賛
返信
1,509件の閲覧回数
keitanagashima
Senior Contributor I

Dear chipexpert,

Thank you for your reply.

I understood that we can't get the GPU drivers source.

But, is it possible to use function of 2D BitBlit without the API's source code?

Best Regards,

Keita

0 件の賞賛
返信
1,510件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, 2D functions can be used please refer to

i.MX_6_G2D_API_User's_Guide.pdf included in

Linux documentation

"L3.10.17_1.0.0_IMX6QDLS_BUNDLE  : Source Code Download Steps Documentation and Demo Images."

i.MX6Q: i.MX 6Quad Family of Applications Processors

Best regards

chip

0 件の賞賛
返信