BitBlit function on GC320 in i.MX6SDL.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BitBlit function on GC320 in i.MX6SDL.

跳至解决方案
2,895 次查看
keitanagashima
Senior Contributor I

Hi.

I'd like to use the BitBlit function on GC320 of i.MX6SDL in Linux.

When using the feature of 2D BitBlit, I think that the Vivante's API must be used.

To use the API of Vivante, the header file of Vivante becomes necessary.

Is it possible to get the source code of the graphics function of Vivante?

Keita

标签 (3)
0 项奖励
回复
1 解答
2,298 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, 2D functions can be used please refer to

i.MX_6_G2D_API_User's_Guide.pdf included in

Linux documentation

"L3.10.17_1.0.0_IMX6QDLS_BUNDLE  : Source Code Download Steps Documentation and Demo Images."

i.MX6Q: i.MX 6Quad Family of Applications Processors

Best regards

chip

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,298 次查看
igorpadykov
NXP Employee
NXP Employee

Freescale does not provide GPU drivers sources because they are license protected.

Sources should be obtained only through local Freescale marketing channel.

0 项奖励
回复
2,298 次查看
keitanagashima
Senior Contributor I

Dear chipexpert,

Thank you for your reply.

I understood that we can't get the GPU drivers source.

But, is it possible to use function of 2D BitBlit without the API's source code?

Best Regards,

Keita

0 项奖励
回复
2,299 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, 2D functions can be used please refer to

i.MX_6_G2D_API_User's_Guide.pdf included in

Linux documentation

"L3.10.17_1.0.0_IMX6QDLS_BUNDLE  : Source Code Download Steps Documentation and Demo Images."

i.MX6Q: i.MX 6Quad Family of Applications Processors

Best regards

chip

0 项奖励
回复