BitBlit function on GC320 in i.MX6SDL.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BitBlit function on GC320 in i.MX6SDL.

Jump to solution
2,133 Views
keitanagashima
Senior Contributor I

Hi.

I'd like to use the BitBlit function on GC320 of i.MX6SDL in Linux.

When using the feature of 2D BitBlit, I think that the Vivante's API must be used.

To use the API of Vivante, the header file of Vivante becomes necessary.

Is it possible to get the source code of the graphics function of Vivante?

Keita

Labels (3)
0 Kudos
Reply
1 Solution
1,536 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, 2D functions can be used please refer to

i.MX_6_G2D_API_User's_Guide.pdf included in

Linux documentation

"L3.10.17_1.0.0_IMX6QDLS_BUNDLE  : Source Code Download Steps Documentation and Demo Images."

i.MX6Q: i.MX 6Quad Family of Applications Processors

Best regards

chip

View solution in original post

0 Kudos
Reply
3 Replies
1,536 Views
igorpadykov
NXP Employee
NXP Employee

Freescale does not provide GPU drivers sources because they are license protected.

Sources should be obtained only through local Freescale marketing channel.

0 Kudos
Reply
1,536 Views
keitanagashima
Senior Contributor I

Dear chipexpert,

Thank you for your reply.

I understood that we can't get the GPU drivers source.

But, is it possible to use function of 2D BitBlit without the API's source code?

Best Regards,

Keita

0 Kudos
Reply
1,537 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, 2D functions can be used please refer to

i.MX_6_G2D_API_User's_Guide.pdf included in

Linux documentation

"L3.10.17_1.0.0_IMX6QDLS_BUNDLE  : Source Code Download Steps Documentation and Demo Images."

i.MX6Q: i.MX 6Quad Family of Applications Processors

Best regards

chip

0 Kudos
Reply