Bit settings file for iMX28EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bit settings file for iMX28EVK

4,119 次查看
x10
Contributor V

Hi, all

 

I try to find the OTP bit seettings file for iMX28EVK to understand the function of those eFuse bits. Thanks in advance.

 

BR

 

 

Cheng Shi

emtronix

0 项奖励
回复
7 回复数

3,230 次查看
admin
Specialist II

OTP Registers

EVKRAW Chip
HW_OCOTP_CUST00x9F0135C00x00000000
HW_OCOTP_CUST10x9F0135C10x00000000
HW_OCOTP_CUST20x000000000x00000000
HW_OCOTP_CUST30x000000000x00000000
HW_OCOTP_CRYPTO00x000000000x00000000
HW_OCOTP_CRYPTO10x000000000x00000000
HW_OCOTP_CRYPTO20x000000000x00000000
HW_OCOTP_CRYPTO30x000000000x00000000
HW_OCOTP_CUSTCAP0x000000000x00000000
HW_OCOTP_LOCK0x000C00000x000C0000
HW_OCOTP_ROM00x000000000x00000000
HW_OCOTP_ROM10x000000000x00000000
HW_OCOTP_ROM20x000000000x00000000
HW_OCOTP_ROM30x000000000x00000000
HW_OCOTP_ROM40x000000000x00000000
HW_OCOTP_ROM50x000000000x00000000
HW_OCOTP_ROM60x000000000x00000000
HW_OCOTP_ROM70x001001000x00100000
HW_OCOTP_SRK00x000000000x00000000
HW_OCOTP_SRK10x000000000x00000000
HW_OCOTP_SRK20x000000000x00000000
HW_OCOTP_SRK30x000000000x00000000
HW_OCOTP_SRK40x000000000x00000000
HW_OCOTP_SRK50x000000000x00000000
HW_OCOTP_SRK60x000000000x00000000
HW_OCOTP_SRK70x000000000x00000000
0 项奖励
回复

3,230 次查看
x10
Contributor V

MfgTool can send data to UUT which will either call fmd's DeviceIoControl to program data into CUST0 or call routines in otp.c to program directly. My imx28 based board is running CE6.0.

Marc coussement said:

How, can we use Mfgtool to program HW_OCOTP_CUST0 OTP register?

 

Marc,
 

0 项奖励
回复

3,230 次查看
MarcCoussement
Contributor I

How, can we use Mfgtool to program HW_OCOTP_CUST0 OTP register?

 

Marc,
 

0 项奖励
回复

3,230 次查看
x10
Contributor V

With the new release 1.6.2.048, the MAC issue should be settled down. Thanks!

0 项奖励
回复

3,230 次查看
StanleyLee
NXP Employee
NXP Employee

BitInit.exe is feasible but not recommended. Mfgtool can do it, too.  You can finish all your work using Mfgtool, this is very important in factory environment.

0 项奖励
回复

3,230 次查看
x10
Contributor V

Thanks for your reply.

I plan to burn the MAC address to HW_OCOTP_CUST0 with tool BitInit.exe one by one at first, and then program the images of eboot.sb and nk.nb0 into my iMX28 based board with MfgTool.

 

BR

 

Cheng Shi

emtronix

0 项奖励
回复

3,227 次查看
ChrisWilliamson
Contributor III

This  is all I could find. Hopefully what you are lookng for is in here somewhere.

 

Chris

0 项奖励
回复