Behavior of i.MX6 DDR Stress Test.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Behavior of i.MX6 DDR Stress Test.

Jump to solution
2,550 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 DDR Stress Test in https://community.freescale.com/docs/DOC-96412.

Please see the attached file.

I understand the stress test tool output a center of delay setting values which can work DDR correctly as attached file (Case A, B).

Then, how about Case C?

The stress test tool can output a suitable setting? or it judge it is NG?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,974 Views
GraceH
Senior Contributor II

Hi Shimoda,

The valid range of DG_HC_DEL is to 0b1101 and DG_DL_ABS_OFFSET is to 0b1111111,

and the total read DQS gating delay is (DG_HC_DEL#)*0.5*cycle + (DG_DL_ABS_OFFSET#)*1/256*cycle.

The suitable delay range can't be out of valid DQS gating delay range.

Grace

View solution in original post

0 Kudos
Reply
1 Reply
1,975 Views
GraceH
Senior Contributor II

Hi Shimoda,

The valid range of DG_HC_DEL is to 0b1101 and DG_DL_ABS_OFFSET is to 0b1111111,

and the total read DQS gating delay is (DG_HC_DEL#)*0.5*cycle + (DG_DL_ABS_OFFSET#)*1/256*cycle.

The suitable delay range can't be out of valid DQS gating delay range.

Grace

0 Kudos
Reply