Behavior of i.MX6 DDR Stress Test.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Behavior of i.MX6 DDR Stress Test.

ソリューションへジャンプ
2,551件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 DDR Stress Test in https://community.freescale.com/docs/DOC-96412.

Please see the attached file.

I understand the stress test tool output a center of delay setting values which can work DDR correctly as attached file (Case A, B).

Then, how about Case C?

The stress test tool can output a suitable setting? or it judge it is NG?

Best Regards,

Satoshi Shimoda

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,975件の閲覧回数
GraceH
Senior Contributor II

Hi Shimoda,

The valid range of DG_HC_DEL is to 0b1101 and DG_DL_ABS_OFFSET is to 0b1111111,

and the total read DQS gating delay is (DG_HC_DEL#)*0.5*cycle + (DG_DL_ABS_OFFSET#)*1/256*cycle.

The suitable delay range can't be out of valid DQS gating delay range.

Grace

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,976件の閲覧回数
GraceH
Senior Contributor II

Hi Shimoda,

The valid range of DG_HC_DEL is to 0b1101 and DG_DL_ABS_OFFSET is to 0b1111111,

and the total read DQS gating delay is (DG_HC_DEL#)*0.5*cycle + (DG_DL_ABS_OFFSET#)*1/256*cycle.

The suitable delay range can't be out of valid DQS gating delay range.

Grace

0 件の賞賛
返信