Are there any test tools to test all of the hardware functions?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there any test tools to test all of the hardware functions?

1,937 Views
charleshuang
Senior Contributor II

We are using imx6 platform which is based on sabresd platform with Yocto BSP.

And we would like test our hardware function,including stress test for CPU,memory,gpu and peripheral devices function like uart、network、usb、display...etc

Are there any test tools to test all of the hardware functions?

Can you recommend satisfy our needs test tool?with or without cost

Or if you want to make a fully hardware function test, how would you recommend to do?

0 Kudos
Reply
4 Replies

1,500 Views
sinanakman
Senior Contributor III

Hi Charles

We have an unannounced internal product in that direction.

Please send me a private e-mail and I'll see if I can

get you more info on this.

Regards

Sinan Akman

0 Kudos
Reply

1,500 Views
charleshuang
Senior Contributor II

You can send e-mail to tim.liang@advantech.com.tw

thanks for your help

0 Kudos
Reply

1,500 Views
sinanakman
Senior Contributor III

Hi Charles, I just sent a follow up e-mail

to the e-mail address you mentioned above.

Please let me know if you haven't received it.

Regards

Sinan Akman

0 Kudos
Reply

1,500 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi charles huang,

So sorry we do not have this test tool to test the hardware functions you mentioned in your thread. In our website only DDR stress test tool provided.

About test all these functions, you can run software on your board to test the functions one by one.

Here I also give you a link abhout i.MX Design&Tool Lists hope it will help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply