Android7 HAL can't open iio:device1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android7 HAL can't open iio:device1

1,052件の閲覧回数
wangvictor
Contributor III

Hi All,

I'm using i.MX6 sabresd for my CPU and the kernel version is 4.4.8.

I'm facing the problem of HAL layer of LightSensor.cpp.

When I try to opendir("/dev/iio:device1")

And it will failed to open.

How can I fix this problem?

Do I need to give more information?

If needed please tell me what else should I give more?

Thanks in Advanced!

ラベル(5)
タグ(3)
0 件の賞賛
返信
1 返信

911件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you using our BSP? Since the kernel versions that you are using is different from the ones that we use in our BSP.

Best Regards,

Diego.

0 件の賞賛
返信