Android7 HAL can't open iio:device1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android7 HAL can't open iio:device1

1,047 Views
wangvictor
Contributor III

Hi All,

I'm using i.MX6 sabresd for my CPU and the kernel version is 4.4.8.

I'm facing the problem of HAL layer of LightSensor.cpp.

When I try to opendir("/dev/iio:device1")

And it will failed to open.

How can I fix this problem?

Do I need to give more information?

If needed please tell me what else should I give more?

Thanks in Advanced!

Labels (5)
Tags (3)
0 Kudos
Reply
1 Reply

906 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you using our BSP? Since the kernel versions that you are using is different from the ones that we use in our BSP.

Best Regards,

Diego.

0 Kudos
Reply