Hi,
I tried to download the source of android Oreo. I was stuck at repo sync fetch error i.e unable to fetch the imx-firmware
The following error it was shown .
remote: Counting objects: 159, done
remote: Finding sources: 100% (506/506)
remote: Total 506 (delta 348), reused 506 (delta 348)
Receiving objects: 100% (506/506), 447.84 KiB | 421.00 KiB/s, done.
Resolving deltas: 100% (348/348), completed with 181 local objects.
From https://android.googlesource.com/platform/external/llvm
d24ead5..6ce38d7 lldb-master-dev -> aosp/lldb-master-dev
56b15eb..de6ad3a upstream-master -> aosp/upstream-master
error: Cannot fetch imx-firmware
warn: --force-broken, continuing to sync
Fetching projects: 100% (596/596)
error: Exited sync due to fetch errors
---------------------------------------------------
------Repo sync failure
-------------------
How to get the imx-firmware file to download .May i know the reason getting repo sync fetching failure . could anyone please help me how to resolve this issue.
Regrads,
Lakshmikanth R.
Hi,
Thank you for the quick response. I will clone the repository if any problems i will get back to you.
Regrads,
R.Lakshmikanth