Android Oreo Repo sync Failure imx-firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Oreo Repo sync Failure imx-firmware

1,924 Views
lakshmikanthr
Contributor III

Hi,

I tried to download the source of android Oreo. I was stuck at repo sync fetch error i.e unable to fetch the imx-firmware

The following error it was shown .

remote: Counting objects: 159, done
remote: Finding sources: 100% (506/506)
remote: Total 506 (delta 348), reused 506 (delta 348)
Receiving objects: 100% (506/506), 447.84 KiB | 421.00 KiB/s, done.
Resolving deltas: 100% (348/348), completed with 181 local objects.
From https://android.googlesource.com/platform/external/llvm
   d24ead5..6ce38d7  lldb-master-dev -> aosp/lldb-master-dev
   56b15eb..de6ad3a  upstream-master -> aosp/upstream-master
error: Cannot fetch imx-firmware
warn: --force-broken, continuing to sync
Fetching projects: 100% (596/596)  
error: Exited sync due to fetch errors
---------------------------------------------------
------Repo sync failure

-------------------

How to get the imx-firmware file to download .May i know the reason getting repo sync fetching failure . could anyone please help me how to resolve this issue.

Regrads,

Lakshmikanth R.

Labels (1)
0 Kudos
Reply
2 Replies

1,479 Views
joanxie
NXP TechSupport
NXP TechSupport

maybe the sever has issue, try to find here

Freescale Public GIT 

0 Kudos
Reply

1,479 Views
lakshmikanthr
Contributor III

Hi,

Thank you for the quick response. I will clone the repository if any problems i will get back to you.

Regrads,

R.Lakshmikanth

0 Kudos
Reply