Android OS License

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android OS License

2,532 Views
joshua_hong
Contributor III

Hi,

do we have to acquire Android OS License (Android 8 or Android 9) if we want to run the Android OS on I.MX6?

Labels (2)
0 Kudos
Reply
3 Replies

2,422 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Joshua Hong,

If you want to run Android on one of NXP’s i.MX6 EVKs and SABRE boards, you may download the available BSPs which include an End User License Agreement, but no further license is needed.

If you plan to run Android on your own i.MX6 application, you may use Android Open Source Project which also comes with its own license agreement.

If you want to include Android on a finished product, however, you would need to contact Google for more information on licensing.

I hope this helps!

Regards,

0 Kudos
Reply

2,422 Views
joshua_hong
Contributor III

Hi Gusarambula,

Thank you for your explanation.

If my client is developing Android OS on I.MX6 on own design board, which one case applies? Is it the own i.mx6 application or the finished product?

Best regard

Joshua

Field Application Engineer

WT Microelectronics Singapore Pte Ltd

2 Serangoon North Ave 5, #05-01 Singapore 554911

Tel : +65 6853 1788 ext: 1067

Mobile : +65 9146 9763

Email : [email protected]<mailto:[email protected]>

Website : www.wtmec.com<http://www.wtmec.com/WT/?lang=en>;

0 Kudos
Reply

2,422 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Joshua Hong,

I would recommend that you contact Google directly to make sure that you use the correct license for your application.

My apologies for the inconvenience.

Regards,

0 Kudos
Reply