Android OS License

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android OS License

2,610件の閲覧回数
joshua_hong
Contributor III

Hi,

do we have to acquire Android OS License (Android 8 or Android 9) if we want to run the Android OS on I.MX6?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,500件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Joshua Hong,

If you want to run Android on one of NXP’s i.MX6 EVKs and SABRE boards, you may download the available BSPs which include an End User License Agreement, but no further license is needed.

If you plan to run Android on your own i.MX6 application, you may use Android Open Source Project which also comes with its own license agreement.

If you want to include Android on a finished product, however, you would need to contact Google for more information on licensing.

I hope this helps!

Regards,

0 件の賞賛
返信

2,500件の閲覧回数
joshua_hong
Contributor III

Hi Gusarambula,

Thank you for your explanation.

If my client is developing Android OS on I.MX6 on own design board, which one case applies? Is it the own i.mx6 application or the finished product?

Best regard

Joshua

Field Application Engineer

WT Microelectronics Singapore Pte Ltd

2 Serangoon North Ave 5, #05-01 Singapore 554911

Tel : +65 6853 1788 ext: 1067

Mobile : +65 9146 9763

Email : [email protected]<mailto:[email protected]>

Website : www.wtmec.com<http://www.wtmec.com/WT/?lang=en>;

0 件の賞賛
返信

2,500件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Joshua Hong,

I would recommend that you contact Google directly to make sure that you use the correct license for your application.

My apologies for the inconvenience.

Regards,

0 件の賞賛
返信