Android JB 4.3 - where is android_usb_fsl.zip?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Android JB 4.3 - where is android_usb_fsl.zip?

跳至解决方案
3,206 次查看
EricNelson
Senior Contributor II

This post refers to a zip-file named android_usb_fsl.zip that contains the device driver for ADB on Windows machines:

Re: i.MX6: Android connect to ADB

Unfortunately, I can't seem to find it in any of the packages in the Android JB4.3_1.0.0-GA release.

标签 (3)
标记 (4)
0 项奖励
回复
1 解答
1,752 次查看
joecrop
Contributor II

In the post you refereed to they require you to get that zip file from the MX53 BSP package.

3. Unpack the Freescale Android USB win driver "android_usb_fsl.zip" in your Android BSP release package. If you can't find this file in your current package, please get the R10.3.x release for i.MX5x and unpack it.

4. File "tetherxp.inf" in the unpacked "android_usb_fsl" may not be the updated one if the "android_usb_fsl.zip" is extracted from an old release. So, please overwrite the file "tetherxp.inf" in unpacked "android_usb_fsl.zip" by the new "tetherxp.inf" in your current Android BSP release.

I got this zip file, replaced the "tetherxp.inf" file from the MX6SL BSP and installed. A new device (Android ADB Interface) now shows up in my device manager but has an error: "This device cannot start (Code 1)" which implies the driver is wrong.

Try downloading the MX53 BSP and let me konw if you have any luck.

So far this is still not working for me.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,753 次查看
joecrop
Contributor II

In the post you refereed to they require you to get that zip file from the MX53 BSP package.

3. Unpack the Freescale Android USB win driver "android_usb_fsl.zip" in your Android BSP release package. If you can't find this file in your current package, please get the R10.3.x release for i.MX5x and unpack it.

4. File "tetherxp.inf" in the unpacked "android_usb_fsl" may not be the updated one if the "android_usb_fsl.zip" is extracted from an old release. So, please overwrite the file "tetherxp.inf" in unpacked "android_usb_fsl.zip" by the new "tetherxp.inf" in your current Android BSP release.

I got this zip file, replaced the "tetherxp.inf" file from the MX6SL BSP and installed. A new device (Android ADB Interface) now shows up in my device manager but has an error: "This device cannot start (Code 1)" which implies the driver is wrong.

Try downloading the MX53 BSP and let me konw if you have any luck.

So far this is still not working for me.

0 项奖励
回复
1,752 次查看
EricNelson
Senior Contributor II

Thanks Joe,

With that, I was able to find the package (whew!).

I don't run Windows, but passed it on to a customer to see if it helps.

We've had lots of other queries from Windows customers who haven't gone through this process.

Under Linux, things just work :smileywink:

0 项奖励
回复