Android Fast Boot on i.MX6 Sabresd Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Fast Boot on i.MX6 Sabresd Board

Jump to solution
4,648 Views
erickang
Contributor II

Dear All,
I want to apply the Fast Boot function into Android.
I'm using the Android jb4.2.2_1.1.0 BSP for i.MX6Q SabreSD board.

I saw the Linux Fast Boot Guide like as below in this Freescale Community.
- Linux Fast Boot on i.MX6Q Board: Building Steps
   . https://community.freescale.com/docs/DOC-94738
- Linux Fast Boot on i.MX6 Sabresd Board
   . https://community.freescale.com/docs/DOC-93619

Based on upper references, I applied the patches into Android jb4.2.2_1.1.0 BSP.
But I couldn't boot faster than the normal boot.

Could you give me any assistance?

Best Regards,
Eric.

Labels (4)
0 Kudos
Reply
1 Solution
2,267 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Eric

     Have you compared the logs of with I/O the fast boot patch? As fast boot's DOC said, there will be some difference after enabling fast boot, so you can see the difference from the log first, see whether the fast boot related changes applied correctly.

View solution in original post

0 Kudos
Reply
1 Reply
2,268 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Eric

     Have you compared the logs of with I/O the fast boot patch? As fast boot's DOC said, there will be some difference after enabling fast boot, so you can see the difference from the log first, see whether the fast boot related changes applied correctly.

0 Kudos
Reply