Android Fast Boot on i.MX6 Sabresd Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Android Fast Boot on i.MX6 Sabresd Board

跳至解决方案
4,644 次查看
erickang
Contributor II

Dear All,
I want to apply the Fast Boot function into Android.
I'm using the Android jb4.2.2_1.1.0 BSP for i.MX6Q SabreSD board.

I saw the Linux Fast Boot Guide like as below in this Freescale Community.
- Linux Fast Boot on i.MX6Q Board: Building Steps
   . https://community.freescale.com/docs/DOC-94738
- Linux Fast Boot on i.MX6 Sabresd Board
   . https://community.freescale.com/docs/DOC-93619

Based on upper references, I applied the patches into Android jb4.2.2_1.1.0 BSP.
But I couldn't boot faster than the normal boot.

Could you give me any assistance?

Best Regards,
Eric.

标签 (4)
0 项奖励
回复
1 解答
2,263 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Eric

     Have you compared the logs of with I/O the fast boot patch? As fast boot's DOC said, there will be some difference after enabling fast boot, so you can see the difference from the log first, see whether the fast boot related changes applied correctly.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,264 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Eric

     Have you compared the logs of with I/O the fast boot patch? As fast boot's DOC said, there will be some difference after enabling fast boot, so you can see the difference from the log first, see whether the fast boot related changes applied correctly.

0 项奖励
回复