Android Fast Boot on i.MX6 Sabresd Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Fast Boot on i.MX6 Sabresd Board

ソリューションへジャンプ
4,658件の閲覧回数
erickang
Contributor II

Dear All,
I want to apply the Fast Boot function into Android.
I'm using the Android jb4.2.2_1.1.0 BSP for i.MX6Q SabreSD board.

I saw the Linux Fast Boot Guide like as below in this Freescale Community.
- Linux Fast Boot on i.MX6Q Board: Building Steps
   . https://community.freescale.com/docs/DOC-94738
- Linux Fast Boot on i.MX6 Sabresd Board
   . https://community.freescale.com/docs/DOC-93619

Based on upper references, I applied the patches into Android jb4.2.2_1.1.0 BSP.
But I couldn't boot faster than the normal boot.

Could you give me any assistance?

Best Regards,
Eric.

ラベル(4)
0 件の賞賛
返信
1 解決策
2,277件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Eric

     Have you compared the logs of with I/O the fast boot patch? As fast boot's DOC said, there will be some difference after enabling fast boot, so you can see the difference from the log first, see whether the fast boot related changes applied correctly.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,278件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Eric

     Have you compared the logs of with I/O the fast boot patch? As fast boot's DOC said, there will be some difference after enabling fast boot, so you can see the difference from the log first, see whether the fast boot related changes applied correctly.

0 件の賞賛
返信