Android 9 Build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 9 Build error

ソリューションへジャンプ
4,901件の閲覧回数
aravinthkumarja
Senior Contributor II

While building Android 9 source code I'm getting below error.

 

ninja: build stopped: subcommand failed. 01:48:30 ninja failed with: exit status 1 01:48:31 Unable to parse ninja entry "\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x0016486\t16651\t1617599514\tout/target/product/iwg33m_8m/vendor/etc/fstab.freescale\t1595fef4c7261bfc": strconv.Atoi: parsing "\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x0016486": invalid syntax #### failed to build some targets (01:00:24 (hh:mm:ss)) #### Plz help to fix.

0 件の賞賛
返信
1 解決策
4,859件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

We recommand using ubuntu 18 to compile android 9

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,883件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Make sure you have installed all host packages ,and follow the user guide.this seem not be  bsp source code error. Some files could be lost when sync, so you can try to resync the source code. 

0 件の賞賛
返信
4,869件の閲覧回数
aravinthkumarja
Senior Contributor II

Once again I installed all packages and repo sync again also. But facing same error.

0 件の賞賛
返信
4,860件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

We recommand using ubuntu 18 to compile android 9

0 件の賞賛
返信