Android 9 Build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Android 9 Build error

跳至解决方案
4,966 次查看
aravinthkumarja
Senior Contributor II

While building Android 9 source code I'm getting below error.

 

ninja: build stopped: subcommand failed. 01:48:30 ninja failed with: exit status 1 01:48:31 Unable to parse ninja entry "\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x0016486\t16651\t1617599514\tout/target/product/iwg33m_8m/vendor/etc/fstab.freescale\t1595fef4c7261bfc": strconv.Atoi: parsing "\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x00\x0016486": invalid syntax #### failed to build some targets (01:00:24 (hh:mm:ss)) #### Plz help to fix.

0 项奖励
回复
1 解答
4,924 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

We recommand using ubuntu 18 to compile android 9

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,948 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Make sure you have installed all host packages ,and follow the user guide.this seem not be  bsp source code error. Some files could be lost when sync, so you can try to resync the source code. 

0 项奖励
回复
4,934 次查看
aravinthkumarja
Senior Contributor II

Once again I installed all packages and repo sync again also. But facing same error.

0 项奖励
回复
4,925 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

We recommand using ubuntu 18 to compile android 9

0 项奖励
回复