Android 7 Bluethooth Stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 7 Bluethooth Stack

2,820件の閲覧回数
jith
Contributor II

Hi,

Which is the Bluetooth stack used in Android 7?

Is it support Bluetooth 5?

ラベル(1)
2 返答(返信)

2,538件の閲覧回数
jith
Contributor II

Thank you so much

0 件の賞賛
返信

2,538件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jith

as Android 7 is based on L4.1.15 kernel one can refer to

sect.55.3.3 Bluetooth Stack attached Linux Manual

Android N7.1.1_1.0.0 Release Announcement 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------