Android 11 Image.zl4 compression issue while building kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 11 Image.zl4 compression issue while building kernel

2,683件の閲覧回数
SL239
Contributor II

Has anyone else encountered this problem while trying to build Android 11 Automotive on Ubuntu for the iMX8 board?

It occurs when I run "./imx-make.sh -j4 2>&1 | tee build-log.txt" and prevents the kernel from being built.

Android 10 builds just fine.

Thanks.

 

MicrosoftTeams-image.png

0 件の賞賛
返信
2 返答(返信)

2,650件の閲覧回数
SL239
Contributor II

So I was able to get around this issue. I was using the IMX8QM board, I was trying to run NXP's 11.0.0_2.4.0_ANDROID_SOURCE with an automotive build configuration. I guess automotive is not supported in this release. I ended up using NXP's automotive_11.0.0_2.3 instead and it built just fine. Thank you.

0 件の賞賛
返信

2,663件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

There are different version of Android Auto BSP.

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-automotive-os-for-i-mx-a...

 

Could you tell me which one are you using?

Which board are you using?

0 件の賞賛
返信