Android 11 Image.zl4 compression issue while building kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 11 Image.zl4 compression issue while building kernel

2,758 Views
SL239
Contributor II

Has anyone else encountered this problem while trying to build Android 11 Automotive on Ubuntu for the iMX8 board?

It occurs when I run "./imx-make.sh -j4 2>&1 | tee build-log.txt" and prevents the kernel from being built.

Android 10 builds just fine.

Thanks.

 

MicrosoftTeams-image.png

0 Kudos
Reply
2 Replies

2,725 Views
SL239
Contributor II

So I was able to get around this issue. I was using the IMX8QM board, I was trying to run NXP's 11.0.0_2.4.0_ANDROID_SOURCE with an automotive build configuration. I guess automotive is not supported in this release. I ended up using NXP's automotive_11.0.0_2.3 instead and it built just fine. Thank you.

0 Kudos
Reply

2,738 Views
jimmychan
NXP TechSupport
NXP TechSupport

There are different version of Android Auto BSP.

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-automotive-os-for-i-mx-a...

 

Could you tell me which one are you using?

Which board are you using?

0 Kudos
Reply