Alternative to 'curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo'?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Alternative to 'curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo'?

ソリューションへジャンプ
2,413件の閲覧回数
djregan
Contributor III

Hello,  I have friends in China who are asking if it is possible to leverage an alternative to the command?...

curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

...which is described in fsl-yocto-L4.1.15_2.0.0-ga revision documentation set, within document 'i.MX_Yocto_Project_User's_Guide.pdf', sub-section 3.2 ('Setting up the repo utility').

 

They are concerned firewalls in China may be blocking them from successfully leveraging this command.

For developers who are blocked from leveraging this command due to firewalls blocking certain sites, does NXP have an alternative procedure that can be proposed?

 

Thanks much in advance!

--DJ Regan

ラベル(1)
1 解決策
2,027件の閲覧回数
b36401
NXP Employee
NXP Employee

They can refer this document:

https://community.nxp.com/docs/DOC-329574

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,027件の閲覧回数
djregan
Contributor III

I will let them know. :smileyhappy: Appreciate it Victor!

0 件の賞賛
返信
2,028件の閲覧回数
b36401
NXP Employee
NXP Employee

They can refer this document:

https://community.nxp.com/docs/DOC-329574

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------