Alternative to 'curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo'?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Alternative to 'curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo'?

Jump to solution
2,402 Views
djregan
Contributor III

Hello,  I have friends in China who are asking if it is possible to leverage an alternative to the command?...

curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

...which is described in fsl-yocto-L4.1.15_2.0.0-ga revision documentation set, within document 'i.MX_Yocto_Project_User's_Guide.pdf', sub-section 3.2 ('Setting up the repo utility').

 

They are concerned firewalls in China may be blocking them from successfully leveraging this command.

For developers who are blocked from leveraging this command due to firewalls blocking certain sites, does NXP have an alternative procedure that can be proposed?

 

Thanks much in advance!

--DJ Regan

Labels (1)
1 Solution
2,016 Views
b36401
NXP Employee
NXP Employee

They can refer this document:

https://community.nxp.com/docs/DOC-329574

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,016 Views
djregan
Contributor III

I will let them know. :smileyhappy: Appreciate it Victor!

0 Kudos
Reply
2,017 Views
b36401
NXP Employee
NXP Employee

They can refer this document:

https://community.nxp.com/docs/DOC-329574

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------