Add a usb hub to a custom i.MX8M-EVKB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add a usb hub to a custom i.MX8M-EVKB

2,264件の閲覧回数
calibronic
Contributor III

Dear NXP community


Please correct me if I'm wrong.I am designing a custom board based on i.MX8M-EVKB reference design. In the MX8M-EVKB schematic, USB2 is connected to a USB 3.0 HOST Type A connector and M.2 connector (WiFi module) via 0R resistors (R926,R927,R1418,R1417), please check the attached pictures. As far as I understand, in some cases in which I want to connect a device to USB3 HOST Type A connector and a device to M.2 connector, I am not able to communicate with both of them at the same time. I am going to use an usb hub to make it possible that use both devices at same time. Please advice me on a compatible usb hub ic with i.MX8M and a reference schematic design and also does it required to do some modifications in software side ?

with regards, 

Saeid 

0 件の賞賛
返信
1 返信

2,181件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-346008  may do some help for you.

0 件の賞賛
返信