Generate rootfs and card image for iMX8M Mini/Nano from SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Generate rootfs and card image for iMX8M Mini/Nano from SDK

1,546 次查看
cedric_starke
Contributor III

Hi to all iMX8M users and administrators,

while the evaluation of the iMX8M Mini and Nano CPU I use the GIT Yocto Sources to generate a card image for the Eval-Kit. For an own Hardware I used this card image and only changed the Kernel and U-Boot.


These two parts I'm able to build from the Kernel and U-Boot GIT Sources. It’s is easy going and fancy to try any changes in both source bases.


Till today I use the card image from the Yocto project build. To compile Kernel and U-Boot I've also generated the SDK, of course.


Now is my question how to generate the rootfs and also an own card image from this SDK without Yocto? I didn't find any manual regarding this issue and no other question/answer in the community. But I think I’m not the first who tries this.

If I take a look into the SDK content it should be possible to do this and maybe, it's just strait forward copy-past the content into a card image.

Did anybody something like this or is there a helpful manual?


Thanks for answers

Best regards

Cedric

0 项奖励
回复
1 回复

1,494 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Sorry we do not supply this, for linux BSP we build it in the Yocto environment. So recommend you to use it.

0 项奖励
回复