Add DDR4 memory up to 8GB on imx8mp
05-11-2023
01:22 AM
2,040 次查看
I have a self-made imx8mp motherboard, the model using DDR4 is: K4ABG165WA-MCWE, the single chip capacity is 32Gb, the main frequency is 3200Mhz, my motherboard uses two chips, but the configuration cannot be completed using MX8M_Plus_DDR4_RPA_v9.xlsx
6 回复数
05-11-2023
02:42 AM
2,026 次查看

NXP TechSupport
Hi @xjy198903,
I hope you are doing well.
Could you please send your RPA file for review?
Thanks & Regards,
Ritesh M Patel
05-11-2023
03:00 AM
2,022 次查看
when the clock cycle freq is setting 3200,the ddr stress test file :
In summary, this tool cannot complete the configuration of Samsung K4ABG165WA MCWE in IMX8MP (DDR, non lpddr)
05-12-2023
02:42 AM
1,991 次查看

NXP TechSupport
Hi @xjy198903,
Please share the schematic of the processor and DRAM interface for review.
Also, 3200 is the data rate. The cycle clock frequency will be 1600MHz.
Thanks & Regards,
Ritesh M Patel