Add DDR4 memory up to 8GB on imx8mp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Add DDR4 memory up to 8GB on imx8mp

2,814 次查看
xjy198903
Contributor IV

I have a self-made imx8mp motherboard, the model using DDR4 is: K4ABG165WA-MCWE, the single chip capacity is 32Gb, the main frequency is 3200Mhz, my motherboard uses two chips, but the configuration cannot be completed using MX8M_Plus_DDR4_RPA_v9.xlsx

0 项奖励
回复
6 回复数

2,800 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @xjy198903,

I hope you are doing well.

Could you please send your RPA file for review?

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复

2,795 次查看
xjy198903
Contributor IV

register_config.png
when the clock cycle freq is setting 3200,the ddr stress test file :

xjy198903_0-1683798945817.png

In summary, this tool cannot complete the configuration of Samsung K4ABG165WA MCWE in IMX8MP (DDR, non lpddr)

0 项奖励
回复

2,764 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @xjy198903,

Please share the schematic of the processor and DRAM interface for review.

Also, 3200 is the data rate. The cycle clock frequency will be 1600MHz.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复

2,761 次查看
xjy198903
Contributor IV

According to the chip manual, I changed the configuration strategy, RSA can meet my needs: 

xjy198903_0-1683884798035.png

 

0 项奖励
回复

2,758 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @xjy198903,

Good to hear that it is working now.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复

2,794 次查看
xjy198903
Contributor IV

the "DDR4 Density per Device (Gb)" can not input 32

0 项奖励
回复