Access qspi partitions in sd boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Access qspi partitions in sd boot

跳至解决方案
1,359 次查看
rans
Senior Contributor I

Hello,

I would please like to verify the following,

We are going to use evaluation board (sabre x solo) which has both sd & qspi.

When we Linux boot from sd , do we have access to qspi partitions ?

I guess that if it is decalred in device tree , then linux can see both storage devices, but I am not sure about it, becuase I don't have the source code yet for the evaluation board.

Is it that sd is  /dev/sdX , and qspi as /dev/mtdX ?

On starting working with the board we shall have more idea I'm sure, but as a prepearation, we just wanted to verify the above.

Thank you,

Ran

0 项奖励
回复
1 解答
1,236 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ran

it is /dev/mtd, some examples can be found in ucl2.xml from mfg tool.

Linux boot from sd , one has access to qspi partitions.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,237 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ran

it is /dev/mtd, some examples can be found in ucl2.xml from mfg tool.

Linux boot from sd , one has access to qspi partitions.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复